2007-06-12 3:54 AM
Overwriting data in the internal flash
2007-06-12 3:07 AM
Hi
I work on the ST10F273M I would like to know if it's possible to overwrite data in the internal flash (without writing '1' in place of '0 ')? for exemple, if there is this data ''0xAAAAFFFF'' written in the internal flash, can i overwrite it with the data ''0xAAAA5555'' ? thank you Nicolas2007-06-12 3:54 AM
Hi nico456,
Yes, it is possible to overwrite data in the internal flash. The principle is to replace ones with zeros. For example, 0xAAAAFFFF can be overwritten by 0xAAAA5555, 0xAAAA4444, 0x88883333 etc... 0xAAAAFFFF can not be overwritten for example by 0xBBBBFFFF. To write 0xBBBBFFFF, the location must be erased before (becomes 0xFFFFFFFF). Hope this was clear, Regards, Najoua.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.