2005-12-15 11:19 PM
2005-12-08 9:24 PM
Hello all
I have a strange problem, I just included the ST library but I got a linker error as below. that happen with RCCU and GPIO with all the functions defined in the Header file of RCCU and GPIO. the error of one of them is: objects\S1D13305.o(.text+0x0): In function `RCCU_Div2Status': .\source\/rccu.h:157: multiple definition of `RCCU_Div2Status' objects\main.o(.text+0x0):.\source\/rccu.h:157: first defined here Any help pls? Regards,2005-12-15 11:19 PM
Actually I did nothing with the project yet, just importing the gpio.h causes that problem. I came over that by changing the ''inline'' functions in the gpio.h into ''static inline''. It works now but am not sure if its safe to do so!
can you advice please? Regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.