2007-07-16 9:55 PM
2007-07-12 5:23 AM
Hello,
I'm trying to flash an ST10F269 from MS-DOS I have used the ST10flasher dll under windows and this works ok - but I need to do the same thing from DOS (it is on an old development system) I have logged the serial commands and replies and need to understand what they mean. Can you give me the source for monitor002.hex or ST10flasher.dll so that I can understand the commands and replies being sent. If not, is there another way to flash the device under DOS? Many thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.