2004-03-14 9:09 PM
2011-05-17 2:35 AM
Hi there!
i've got a problem with the MFT0. i just want to measure the duration auf a signal, which comes about 50times a second. the MFT0 is programmed with: trigger on T0INA, Clear on Capture, IT for Capture enabled. DMA not enabled. But the Capture-IT will be called to often, while the Capture-Event occures rare. when the capture occures, the count-value is ok, when no signal is connected, the overflow-IT occures - this is all correct so far. but why is the capture-IT called so often, with no Flag (T_FLAGR & Tm_cp0) set? I don't know were the problem is. can anybody help me? thanks. siggi ----------------------- here is the listing: --------------------------- snip void INIT_MFT(void) { // Disable IT di(); spp(T0D_PG); T_PRSR =2; // Value of the prescaler T_REG0R = 0x8000; // Initial value of the counter T_REG1R = 0x8000; T_TCR = Tm_ccp0 | Tm_udc; // Clear on Capture, Direction=Up T_TMR = Tm_rm0 | Tm_ren; // Capture on REG0R, Disable Retrigger T_ICR = Tm_exa_r | Tm_ab_ti; // TxINA=rising, Function=Trigger / IO T_OACR = bin(1,1,1,1,1,1,0,0); // Disable Outputs T_OBCR = bin(1,1,1,1,1,1,0,0); T_CMP0R = 0xf000; /* Initial value of Compare0 register */ T_CMP1R = 0xf000; /* Initial value of Compare1 register */ // Init II spp(T0C_PG); T0_IVR = 0x40; // IT vector T0_IDCR = 0; // Set priority spp(T0D_PG); T_IDMR = Tm_gtien | Tm_cp0i | Tm_oui; // Global IT mask for the MFT T_FLAGR = 0; // clear previous requests (=errors) ei(); // Start MFT T_TCR |= Tm_cen; } #pragma INTERRUPT INT_MFT0_OVER 10 void INT_MFT0_OVER(void) { debug2++; spp(T0D_PG); T_FLAGR &= ~Tm_ouf; }; #pragma INTERRUPT INT_MFT0_CAPT 11 void INT_MFT0_CAPT(void) { spp(T0D_PG); if ( (T_FLAGR & Tm_cp0)==Tm_cp0 ) { // Capture 0 occured debug3++; count[index]=T_REG0R; index++; if (index > 4) index=0; T_FLAGR &= ~Tm_cp0; } else { // Anything else occured !? debug4++; }; };2011-05-17 2:35 AM
Hello There,
You say you are using the MFT for measuring the duration of pulse so you are using the timer in triggered mode, but you also get an overflow interrupt without the trigger. whis is strange since in trigger mode the timer is running only when we have a trigger on the input PIN so check your configrations and try running it on Emulator.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.