2007-04-27 9:35 PM
Memory mapping - running code from internal RAM
2007-04-12 12:04 PM
Hi there,
My code size is much smaller to fit into RAM. Hence, I want to ran the entire code from RAM by copying all code from Flash to RAM. I learned that I can achieve that by using adding this line, The line, * (InRoot$$Sections). I've got the memory map configured accordingly, please refer below for details. However, the code seems to be not working properly after __main. Can someone pleas advise. Thanks in advance. myFlash.scf USER_MODE 0x40000000 0x40000 ; Load Region { FLASH 0x40000000 ; Execution Region { ;71x_vect.o (Vect, +First) ; Uncomment this if Vector is placed in Flash( comment the corresponding RAM Line ) 71x_init.o (Init, +First) * (InRoot$$Sections) ;* (+RO) } ; built-in RAM = 64kBytes RAM 0x20000000 0x10000 { 71x_vect.o (Vect, +First) ; Uncomment this if Vector is placed in RAM( comment the corresponding FLASH line ) * (+RO) * (+RW) * (+ZI) } ; Heap will grow just above ZI region : ; This Symbol is exported to ''71x_init.s'' file HEAP +0 EMPTY 0x400 { } ; Stack Base address exported to ''71x_init.s'' file ( Top of SRAM ) STACK 0x2000F000 EMPTY -0x0 { } }2007-04-22 7:38 AM
Hi vibnwis,
I have the same issue with few particular programs. The execution hangs at a decompress stage after the branch to __main and before the execution of the main(), it seems a bug/ limitation of RVDK linker. I think that you have to escalte the issue to ARM // www.arm.com. Rave :-Z [ This message was edited by: Rave on 22-04-2007 20:10 ]2007-04-27 9:35 PM
Hi Ravi,
You are absolutely right about the bug. ST has confirmed that is a bug, but only fixes it in MDK3.1 which is a new release. Bad news is you need pay for that, almost half of a new product. Incidentally, why should I pay someone for the bugs he introduced. Hope these help.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.