2004-03-18 12:58 AM
2003-10-03 9:50 PM
Hi,
are there some max-write cycles to write data into the EEPROM. Someone told me, that the write cycles are limited because the adressed memory cell can get fail after a lot of write cycles. I would use the EEPROM to save severals data i.e. run time, last operator choice and so on. I couldn't find anything about max write cycles in the data sheet. Who knows about this? Thank's for your help.2003-10-05 9:17 PM
Yes,there is a limit on the write cycles to write data into EEPROM.The Maximum write cycle limit is 300K (minimum) and 1 million cycles(typical).
2004-03-09 11:44 PM
When the datasheet states maximum number of write cycles, is this maximum number of write cycles on a particular cell, or page or per device.
In my application i wanted to increase the maximum number of write cycles by distributing the write over a number of eeprom locations. Will this work?2004-03-18 12:58 AM
The guaranteed write/erase cycles specificed by the datasheet is for each EEPROM cell.
Yes, you can increase the maximum number of write cycles by distributing the write over a number of eeprom locations.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.