2016-08-31 1:43 PM
I have created a new post because I cannot reply on the first one due to functionality of your website.
The problem again :I have used
Viper06X (30KHz) as a buck to get 9V output
, with no load I have the right output voltage. But
when I connect any load (even it is light) the output voltage drops
.
As the load resistance decreases the output voltage decreases !!
It reached 7.8VDC with only 90mA load !!
And it reaches 2.5VDC when the output current tries to reach 150mA !!!
/analogsimulator/flex_app/bin/smps_app_acdc_design.html?msg=%7b%22data%22%3a%7b%22application%22%3a%22acdc%22%2c%22specs%22%3a%7b%22input%22%3a%7b%22v%22%3a%7b%22min%22%3a110%2c%22max%22%3a235%7d%2c%22f%22%3a50%7d%2c%22ic%22%3a%22VIPER06XS%3abuck%22%2c%22output%22%3a%5b%7b%22v%22%3a9%2c%22i%22%3a0.33%2c%22r%22%3a2%7d%5d%7d%7d%2c%22action%22%3a%22new_design%22%7d
#viper06x
2016-09-04 11:58 PM
Please, could you send some wave forms about the current and the output voltage trend?
Otherwise it's impossible to understand which is the problem.2016-09-08 3:15 PM
Ø£Here is a link
http://imgur.com/a/HoftP2016-09-08 11:32 PM
Hello Ahmed,
please could you send an archive of the OrCAD project you are simulating?Best Regards,Carmelo2016-09-21 5:12 AM
here is a link
https://drive.google.com/open?id=0BydjomGbJ22Namw5eUt5YjJOWjA2016-09-22 5:18 AM
Hello,
the application you sent me is not correct. For example it contains a very small output capacitance (C4=1nF) and the resistor R2 is not connected well.
Please find attached a solution designed with eDesign Studio ready to be simulated.
Best Regards,
Carmelo
________________ Attachments : VIPER06.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzEO&d=%2Fa%2F0X0000000bIf%2FQSBoSaBYl8uIae1wlVHtt4ILJYXMwNXKO27Nb_VjMZE&asPdf=false2016-09-24 3:58 AM
Thanks C
armelo,
Yes you are right I have problem with the files .Seems also that I have a problem in my OrCad A/D simulation, if you can send me a screenshot of sweep analysis I will be thankful.2016-09-25 10:57 PM
Hello,
can you please provide me further details about the simulation you would like to run? The kind of sweep analysis, the simulation settings, the waveforms you want to analyze.
Best Regards
Carmelo
2016-09-27 10:50 AM
I just want the output voltage variation with varying the load resistance , so it is only the VI curve needed .
Thanks Carmelo for your friendly support .We’re moving the ST Community to a new platform to give you a better and more reliable community experience.