2005-01-03 4:20 AM
linking error using HIware compiler
2004-12-30 2:57 AM
Hi all
i am pasting the output i am getting while i am compiling the code . i am getting the error as follows anybody to help me out bye WARNING L2300: Segment STACK_SEG not found in any objectfile Reading initialization information ... Allocating objects ... ERROR L2009: Out of allocation space in segment BUFFER1_EP2_512 at address 1A502005-01-03 4:20 AM
Have you insert STACKTOP?
Example for ST7LITE 9, file project.prm: /* * FILE project.prm * ST7FLITE09 */ LINK project.abs NAMES main.o isr.o funcs.o END SECTIONS MY_ZRAM = NO_INIT 0x0080 TO 0x00FE; /* Le prime due locazioni di EEPROM contengono RCCR0 e RCCR1 */ MY_EEPROM = NO_INIT 0x1000 TO 0x107F; /* L'area di ROM si limita a FFDC (seguono RCCR0, RCCR1 e i vettori) */ MY_ROM = READ_ONLY 0xFA00 TO 0xFFDC; PLACEMENT DEFAULT_RAM, _ZEROPAGE, _OVERLAP INTO MY_ZRAM; DEFAULT_ROM, ROM_VAR, STRINGS INTO MY_ROM; NV_VAR INTO MY_EEPROM; END STACKTOP 0x1FF INIT main VECTOR ADDRESS 0xFFE0 DummyISR /* not used */ VECTOR ADDRESS 0xFFE2 DummyISR /* SPI */ VECTOR ADDRESS 0xFFE4 RTCISR /* LITE TIMER RTC1 */ VECTOR ADDRESS 0xFFE6 DummyISR /* LITE TIMER IC */ VECTOR ADDRESS 0xFFE8 DummyISR /* AT TIMER OVERFLOW */ VECTOR ADDRESS 0xFFEA DummyISR /* AT TIMER OC/IC */ VECTOR ADDRESS 0xFFEC DummyISR /* AVD */ VECTOR ADDRESS 0xFFEE DummyISR /* not used */ VECTOR ADDRESS 0xFFF0 RTC2ISR /* LITE TIMER RTC2 */ VECTOR ADDRESS 0xFFF2 DummyISR /* EI3 */ VECTOR ADDRESS 0xFFF4 DummyISR /* EI2 */ VECTOR ADDRESS 0xFFF6 DummyISR /* EI1 */ VECTOR ADDRESS 0xFFF8 DummyISR /* EI0 */ VECTOR ADDRESS 0xFFFA DummyISR /* AWU */ VECTOR ADDRESS 0xFFFC DummyISR /* TRAP, not maskable */ VECTOR ADDRESS 0xFFFE main /* RESET, not maskable */We’re moving the ST Community to a new platform to give you a better and more reliable community experience.