2004-02-10 1:44 AM
2011-05-17 2:58 AM
I notice in your examples for the DK3200 PortA (peripheral mode) is used for lcd data.
In the past I have used P0 (address/data) for lcd data - this method was also used on the DK900 dev boards - is this possible with the uPSD. I cannot see any reason why not but thought I would check here before I try it. This would then free PortA for GPIO. Many Thanks sjo2011-05-17 2:58 AM
According to page 47 of the uPSD 323x data sheet,
(http://www.st.com/stonline/books/pdf/docs/9188.pdf), Port 0 and Port 2 are dedicated external address and data bus and can NOT be used as GP I/O or Peripheral I/O mode.2011-05-17 2:58 AM
I know they are dedicated, as they are on all 8051 with external memory.
My question is can a upsd be attached to an lcd on p0 as the DK900 kit was. I have attached schematic of what I mean. Regards sjo2011-05-17 2:58 AM
As I said before attaching an lcd to P0 is quite common on the 8051 world so I thought I would try it anyway.
I have done this on the DK900 kit with an 8031 attached. It can be done and works very well. I have attached the code so everyone else can use a lcd on P0, thus saving a port. The only improvements is to use either PA or PB (bits 0,1) for the RS and RW lines , this would save having to use the cpld. Simply write 0x03 to the CONTROL register (address out) and set the DIRECTION as output - this can be done at runtime. Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.