2025-05-28 6:43 PM - last edited on 2025-05-29 12:44 PM by Peter BENSCH
Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).
Hello, I am having a problem reading the technical manual related to the L9945. The manual ‘Charge Pump Stress Estimation in Switching Applications’ mentions that the e ST L9945 Charge Pump Stress Calculator is attached to the document. However, I cannot find it in the PDF file. Can you provide me with a download location for the ST L9945 Charge Pump Stress Calculator?
2025-05-29 12:53 PM
You are talking about the application note AN5074: Charge pump stress estimation in switching applications, which actually contains the Excel sheet itself. Your PDF reader should have a tools bar at the top left or bottom left where you can switch the view to Thumbnails or Outline. You should also see a button with a Paperclip there, which you can click to see the attachment and save it locally. The attachment has the file name:
L9945 Charge Pump Stress Calculator.xlsx
Hope that helps?
Regards
/Peter
2025-05-30 1:12 AM
First of all, thank you very much for your answer. It exactly addressed my question. However, during the actual operation, I didn't find the icon you mentioned. I wonder if there is a specific reader requirement or if you could just email the file to me directly.
Thank you again for your help.
Regards
/Piper
2025-05-30 9:37 AM
What operating system and which PDF viewer are you using?
2025-06-03 9:59 PM
Win operating system, Google Chrome
2025-06-30 2:02 AM
I have just looked again with the Chrome browser, where I also cannot find an attachment. Apparently Google has not implemented this.
So please download the PDF to your local computer and open it with a proper PDF viewer and not with this strange Chrome browser.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.