2019-09-24 4:25 AM
void main(void)
{
float temperature = 0;
const float Rp=10000.0; //10K
const float T2 = (273.15+25.0); //T2 298.15
const float Bx = 3380.0; //B
const float Ka = 273.15;
float Rt = 0;
//double d_num = 0;
float ln_value = 0;
int tmp_int1 = 0;
int tmp_int2 = 0;
float tmp_frac = 0;
int record_cnt = 0; // record counter
//uint16_t read_cnt = 2;
//short int rd_data = 0;
uint16_t k_addr = 0;
//write to eeprom temperature
CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_8);
//CLK_GetClockFreq(void)
//GPIO_Init(GPIOA, GPIO_Pin_2, GPIO_Mode_Out_PP_Low_Slow); // for test
//TIM1_Config();
LCD_Cmd(DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);
RTC_Config();
//ADC1_setup();
//PE7
while(1)
{
RTC_SetWakeUpCounter(SAMPLE_TIME * 60);
RTC_WakeUpCmd(ENABLE);
LCD_Cmd(DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);
//TIM1_Cmd(DISABLE);
//TIM1_SetCounter(0);
//sEE_DeInit();
//printf(VERSION);
//PWR_UltraLowPowerCmd(DISABLE);
halt();
RTC_WakeUpCmd(DISABLE);
//RTC_ClearITPendingBit(RTC_IT_WUT);
}
}we measure 70-80uA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.