2008-03-05 11:15 AM
Is this another Bug in the NEW FWLib for the SSP?
2011-05-17 2:32 AM
Where is SSP1? Comment says 0 or 1
Where are the Code reviews? With all these bugs we should get free support forever! Motorola gave me free support many years ago for finding many of their bugs! /******************************************************************************* * Function Name : SSP_DeInit * Description : Deinitializes the SSPx peripheral registers to their default * reset values. * Input : SSPx: where x can be 0 or 1 to select the SSP peripheral. * Output : None * Return : None *******************************************************************************/ void SSP_DeInit(SSP_TypeDef* SSPx) { if(SSPx == SSP0) { /* Reset the SSP0 registers values*/ SCU_APBPeriphReset(__SSP0,ENABLE); SCU_APBPeriphReset(__SSP0,DISABLE); } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.