2005-08-25 10:30 PM
2005-08-18 10:43 PM
I am new on the STR7 uC and just start programming it. I do understand the IRQ mechanism in general. I have a question about the IRQhandler. I am looking for some kind of a service routine that handles IRQ's of the same priority at the same time.
I read something about a PPP_IRQhandler in AN1776.pdf but I could not find enough information to understand it. Does someone have more information about this? Thanks,2005-08-22 3:37 AM
Thanks for the document, together with the datasheet I do understand the priciple now. But I still have difficulties implementing it in my software.
What I want is an period interrupt from timer 1 and an interrupt that sample one of channel one of the ADC is ready. The timer interrupt alone and the ADC interrupt alone are working. But if I put them together only one is working. I gave both the interrupts the same interrupt priority(1). If every- thing is right and both interrupts are happening at the same time ADC interrupt is seviced fisrt and than the Timer0 interrupt. isn.t it? Does somebody have a simple example program that handels two or more interrups(at the same time). thanks, I tried in software but Thanks,2005-08-25 10:21 PM
Yes now it is working! Thanks a lot!!
Regards, JimmeyWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.