2005-07-12 2:48 AM
2005-07-09 9:34 AM
This is from my Keil Compiler documentation.
Do not use the IEN bit in the PSW to disable interrupt. If you set IEN to 0, the PSW gets updated two instruction later. During this time, if an interrupt occurs, the interrupt system is blocked for the entire interrupt function and not just for the C statements you are trying to protect. Is there an Application Note on the in and outs of disabling interrupts on the ST10F269? Will this code work? ATOMIC #03H BCLR IEN NOP NOP2005-07-11 8:16 PM
Hello,
Please refer to the following link:http://www.keil.com/support/man/docs/c166/c166_xf_interrupts.htm
Yes, your code works. Regards,2005-07-12 2:48 AM
Is there no detailed documentation on ST10F269 interrupts? The Keil link leaves the impression that there is some problem with using IEN. The Keil solution does not address the problem of not knowing the interrupt level before interrupts are disabled and then restoring it after.
:-?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.