2003-05-22 7:30 AM
2011-05-17 2:54 AM
hi,
I need some more information regarding the interrupts triggering in the uPSD3200 . I don't know if INT0 and INT1 are triggered by positive level/edge (refer to page 38 of the uPSD321x data sheet ) or they're triggered by negative level/triggered ( refer bit IT0 of the register TCON at the table37 of datasheet). Thanks in advance for any comments. Regards, Jokin2011-05-17 2:54 AM
Hi,
According to Table 37, when IT0 bit is SET, INT0 is triggered at the falling-edge. When IT0 bit is CLEARED, INT0 is triggered at the low-level. IT1 control bit works the same way for INT1.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.