2008-03-05 12:27 PM
2011-05-17 12:50 AM
Hi
I have problem to make any interrupt to work. I tried many sample codes, but none of them work. CODE for external interrupt P3.2 SCU_APBPeriphReset(__VIC, DISABLE); SCU_APBPeriphReset(__WIU, DISABLE); SCU_APBPeriphReset(__GPIO3, DISABLE); SCU_APBPeriphReset(__RTC, DISABLE); SCU_AHBPeriphClockConfig(__VIC, ENABLE); SCU_APBPeriphClockConfig(__WIU, ENABLE); SCU_APBPeriphClockConfig(__GPIO3, ENABLE); SCU_APBPeriphClockConfig(__RTC, ENABLE); WIU_DeInit(); WIU_InitTypeDef WIU_InitStructure; WIU_Cmd(ENABLE ); WIU_ClearITPendingBit(WIU_Line26); WIU_StructInit(&WIU_InitStructure); WIU_InitStructure.WIU_Line = WIU_Line26 ; WIU_InitStructure.WIU_TriggerEdge = WIU_FallingEdge ; WIU_Init(&WIU_InitStructure); // Select WIU line 26 as VIC1.10 interrupt source SCU_WakeUpLineConfig(26); VIC_DeInit(); // Initialize VICs Default vector address registers VIC_InitDefaultVectors(); // Configure the External interrupt group 0 priority VIC_Config(EXTIT0_ITLine, VIC_IRQ, 0); // Enable the External interrupt group 0 VIC_ITCmd(EXTIT0_ITLine, ENABLE); //#################### BUTTONS #################### // Configure PORT3 lines in Input Push-Pull mode GPIO_DeInit(GPIO3); GPIO_StructInit(&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_Init(GPIO3, &GPIO_InitStructure); //buttons normally HIGH ######################################################## Another example for RTC: RTC_DeInit(); RTC_PeriodicIntConfig(RTC_Per_2Hz); RTC_TamperCmd(DISABLE); RTC_AlarmCmd(DISABLE); RTC_ITConfig(RTC_IT_Per, ENABLE); RTC_ITConfig(RTC_IT_Alarm, DISABLE); RTC_ITConfig(RTC_IT_Tamper, DISABLE); RTC_ClearFlag(RTC_FLAG_Per|RTC_FLAG_Per|RTC_FLAG_Tamper); VIC_DeInit(); VIC_Config(RTC_ITLine, VIC_IRQ, 1); VIC_ITCmd(RTC_ITLine, ENABLE); ///////////// The same with Timers.... No IRQHandler() is called... for any source! This is a part of bigger project... Maybe I forgot about some configuration or there is special action needed in CrossWorks... Has anybody some examples working with CrossWorks 1.7 Sorry for english2011-05-17 12:50 AM
I found solution...
__ARMLIB_enableIRQ(); // Enable gloabal Interrupts Thats what I missed... It wasn't explained anywhere! Now it works :DWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.