2005-12-26 8:54 PM
2005-12-25 4:42 AM
Hi!
I have a question about using interrupts in Boot Loader program. I have MCU – ST72561 High Density Flash Memory – 60kB IAP(In Application Programming) The purpose of boot loader (from sector0) is programming of sectors 1 and 2 with new program. Boot loader code and the interrupt vectors resides in the write protected sector 0. Sector0 will never be changed again, although sector1 and sector2 can have many revisions (for new program). //////////////////////////////////////////////////////////////////////// A question is –Can I use the same interrupts (for example: Can Bus Interrupts or timer8 or timer16 interrupts) also in my Boot Loader program (in sector 0 of HDFlash which is write protected) and also in new program (in sector1 and 2 of HDFlash Which is NOT write protected) ? What can I do ? Not make use of any interrupt in Boot Loader program? To provide mechanism to use any of the interrupts in new program? How can I do this? What happens to address of interrupt vector if I want to use that interrupt initially in boot loader and later in new program? Report this post to a moderator [ This message was edited by: sergeyna on 25-12-2005 18:13 ] [ This message was edited by: sergeyna on 25-12-2005 18:14 ] [ This message was edited by: sergeyna on 26-12-2005 06:59 ] [ This message was edited by: sergeyna on 26-12-2005 08:26 ]2005-12-26 8:54 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.