2005-12-05 8:30 PM
Information needed on STANDBY mode
2005-07-22 6:07 AM
Hi all,
There are a few things I'm not sure about regarding STANDBY mode. The datasheet says ''All the I/Os belonging to the kernel are forced into High Impedance''. Does that mean ALL I/O pins, or are there exceptions (e.g. EMI, pins configured as Alternate Functions, etc.) ? Also, it says that the system RAM is cleared. What happens to the internal registers ? Do they all retain their values, or are some reset to the default values (e.g. I/O pins config, clock config...) ? Basically, I want to be able to power-down my system by software, and restart it with the WAKEUP pin. I'm thinking about doing the following : * On power-down : - switch to the 32 kHz oscillator - power-down my external oscillator (connected to the CK pin) - activate the STANDBY mode * On wake-up : - switch back to the external oscillator - restart the program Is this going to work as expected ? Any info will be greatly appreciated ! :D2005-07-26 12:38 AM
Hello,
The STANDBY sequence is initiated either: – by setting the PWRDWN bit in the PCU_PWRCR register (software STANDBY entry) – or by externally forcing the nSTDBY pin to ‘0’ (hardware STANDBY entry). Caution: You have to manage the nSTDBY, WAKEUP and RESET pin states in order to enter or exit STANDBY mode (refer to the STR71x reference manual, STANDBY section). Cheers Hich ;)2005-07-26 1:45 AM
Hi Hich,
Thanks for your reply. I understand how to initiate standby mode (I'll be using the software entry), but I'm still not sure about the high-impedance thing, and whether all registers values are preserved when restarting from standby. I'm currently designing a protoype board, and I'll like to be sure that my understanding is correct before finalizing the PCB :)2005-07-26 1:50 AM
Hi Fizlo,
Core, memories and peripherals not powered by 1.8V internal supply. Cheers, Hich :D2005-07-26 2:02 AM
Sorry to bother you again Hich,
So if I understand correctly your reply, - All I/O pins switch to high-impedance - All registers values are preserved - Only the RAM is cleared Right ? 8-)2005-07-26 2:09 AM
Hi,
Right, just All I/Os are forced to high impedance except the Standby I/Os(nSTDBY, nRSTIN, WAKEUP, RTCXTI and RTCXTO.). ciao, hich2005-07-26 2:29 AM
Thank you very much, Hich ! :D
2005-07-27 9:46 PM
Hi,
You are welcome. Cheers, Hich :p2005-12-05 8:30 PM
Hi,
After wake-up from the standby mode only the RTC data are preseved, RAM and all the others peripherals data are cleared. Best regatds, Hich 8-)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.