2003-08-04 1:15 AM
2003-08-03 2:53 AM
Hello
In the Softecmicro - Indart program there is an option for Emulator , I want use it but there is only 2 options -> LPT1 and 2 . Where is the USB ? Latino2003-08-03 9:03 PM
What kind of inDART model do you have? The code is placed in the board.
For inDART based on USB communication, no port settings are required. You have only to select the correct hardware model code in the communication Settings dialog box. --Piero2003-08-03 9:56 PM
Hello
I intall the Softec Indart for the ST7lite and the OS ask me for a driver for the USB and i don't have it . Where i can find it ? Latino2003-08-04 1:15 AM
You must first install the software, and THEN plug the inDART unit to the PC. Windows will automatically recognize the instrument.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.