2003-03-02 9:43 PM
inDART-ST7/521 kit : can not get out from the Cosmic startup file, crtsx.s
2003-02-12 9:26 AM
I have an inDART-ST7/521 kit configured to target a ST72521R9T. At first, I used V1.05 then I recently switched to V1.0.9.
For both versions, I noticed that my ST72521 program was sometime stuck in the crtsx.s startup file (I use Cosmic). Other times, I have some communication errors using STVD and Data Blaze. I am sure of my Cosmic code because I have tested it on a ST7 EMU3 emulator. My Indart kit is also brand new. Any idea to explain these 2 issues ? Jojo2003-03-02 9:43 PM
When you say you're stucked in the startup file, does that mean stuck on a particular source code line or stucked because of a reset for instance? Check if you're configured in H/W WDG for instance (or place a breakpoint on the first line of the startup to see if the program performs reset).
Do not hesitate also to ask support from Cosmic or Softec!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.