2006-07-17 8:07 PM
2006-07-14 3:27 AM
Hi,
I'm working with ST72F264 micro. In my application PA0, PA1 are used as outputs connected to transistors. When I burn the micro everything works ok but when I try to debug using InDART-STX I get ''communication error....'' when I press the ''!'' RUN button. When I define these pins as inputs I can debug normally. Is it allowed to define PA0, PA1 as outputs when debugging? Thanks2006-07-17 8:07 PM
Hi Gilat,
During the no-chip debug mode, command-based protocol via the ICCDATA(PA1) and ICCCLK (PA0) lines to communicate with the microcontroller, andfor this reason, both I/O will be reserved. Sothe application should not use (define) these I/O during debugging session. If you really need to use PA0 and PA1 for your spplication, you have to inactivate the code on PA0 and PA1.and then test and debug these ports by stand alone the application (not using inDART-STX for debugging these ports) :DWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.