2006-02-20 7:51 PM
2006-02-13 8:32 PM
I am using IAR 430A Kickstart to debug my str710 board.
I want to download the example program to ext sram 0x62000000. But when I download the program, It can go to main as flow: --- Now branches to a C lib function b ?main ; Note : use B not BL, because an application will ; never return this way But when I step to go.It can't go to my main function. I don't know why [ This message was edited by: dom on 14-02-2006 10:15 ] ________________ Attachments : lnk_ext_ram.xcl : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtIL&d=%2Fa%2F0X0000000aLC%2FaJXLryWiqycvIYhSSd_QRMqWC7.jlqMJbvfrYZu6jfs&asPdf=false2006-02-14 11:50 AM
Yes,I have initialize EMI using the same macro.
But when I download the program to 0x20000000,It works well. When I download the program to 0x62000000, It can't go to main function.2006-02-19 8:26 PM
No,I don't know why.
My project is just the ST Lib example. I link it to 0x20000000 It works well. But I link it to ext sram 0x62000000,It can't go to main.2006-02-20 1:30 PM
How can I download my program to EXT.SRAM?
My board has a ISSI SRAM IS61LV25616-10T using CS1 pin. But I can't download my program to 0x62000000. I am using ADS.[ This message was edited by: dom on 21-02-2006 03:01 ]2006-02-20 7:51 PM
Hi Zouh,
I am sorry.It can't work. Maybe my board is something wrong.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.