2003-04-02 3:50 AM
2011-05-17 2:33 AM
Can we make IAP on the ST92F150 with the RS232 ?
2011-05-17 2:33 AM
Yes. Using RS232 or other serial communication (CAN, SCI etc.).
The AN1275 (In-Application Programming for the ST92F120) has the drivers you are looking for : updating the Flash and EEPROM memory by receiving a standard Intel® hex file via a RS-232. It can be easily ported to the ST92F150. Other useful links : - AN977 : Guidelines for upgrading from the ST92F120 (0.50 ¦m) to the ST92F124/F150/F250 (0.35 ¦m) - ''Simple program example?'' discussion from the ST9 forum Ciao Skywalker2011-05-17 2:33 AM
Is there an option to make IAP with the I2C ?
2011-05-17 2:33 AM
You can use any communication protocol and this includes I2C.
Just replace the communication drivers in AN1275 by the I2C ones. FYI, I2C drivers can be found the ''ST9+ I2C'' discussion. With or without DMA access. SkywalkerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.