2007-03-09 5:51 AM
2007-03-08 4:42 AM
Are there any examples of an interrupt driven I2C read (using restart)?
I actually need to do multiple read-write sequences from interrupts. I saw a previous post and the write was interrupt driven, but the reads were sequential code. Thanks Jon O'Donnell NuVo Technologies2007-03-09 5:51 AM
I've used interrupt-driven I2C IO to interface the ADS7823 which is an ADC. It happens to use repeated START as well. See if you find the file useful.
Regards, - mike ________________ Attachments : adc.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtGU&d=%2Fa%2F0X0000000aKr%2FzvLCAwYBqbUzgjAcOMzVmuCDYRSURPSTfx.IYdlozq4&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.