2009-03-03 10:06 PM
2011-05-17 12:57 AM
Hi all
I want to Interface I2C memory eith Str912FAW44. In datasheet it is given that EVF and BTF bits are set by hardware with an interrupt if the ITE bit is set. But in example1 of I2C no interrupt is enabled and it is checking for events.I am also doing the same. But Event flag is not set. Program is not able to receive I2C_EVENT_MASTER_MODE_SELECT event after generating start Bit. I2C_EVENT_MASTER_MODE_SELECT event is not set. Does anybody know the solution ,please let me know. Regards Sai2011-05-17 12:57 AM
Hi all
Same prog works(Busy get set) with port2.0 and 2.1 Regards SaiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.