2025-08-27 3:28 AM
Hi everyone: i received in these days a custom PCB i designed based on the STM32F411 microcontroller:
I wanted to experiment with such MCUs and make a custom board with them for the first time; i was also interested in making it compatible with the arduino framework through PlatformIO as i am already experienced with that environment.
I started running some tests and i turned out that i was able to program it in DFU mode and to use the serial monitor just fine; however the problems started when i tryed to use I2C sensors like this BME280 Breackout board i got from Amazon: i started simple by connecting it up to 3V3, same GND ans the STM32 board, and SDA and SCL according to the attached PCB schematic.
I also used this code in the platformio's main.c file:
#include <Arduino.h>
#include <Wire.h>
int nDevices = 0;
void setup() {
Wire.begin(PB7, PB6);
Serial.begin(115200);
delay(100);
pinMode(PC13, OUTPUT);
Serial.println("I2C pronto!");
// Scan I2C
byte error, address;
for (address = 1; address < 127; address++) {
Wire.beginTransmission(address);
error = Wire.endTransmission();
if (error == 0) {
Serial.print("Device found on 0x");
Serial.println(address, HEX);
nDevices++;
}
delay(5); // Add small delay between attempts
}
}
void loop() {
if(nDevices != 0){
digitalWrite(PC13, !digitalRead(PC13));
delay(1000);
} else {
Serial.println("No I2C Device Found");
delay(1000);
}
}and this in the platformio.ini file:
; PlatformIO Project Configuration File
;
; Build options: build flags, source filter
; Upload options: custom upload port, speed and extra flags
; Library options: dependencies, extra library storages
; Advanced options: extra scripting
;
; Please visit documentation for the other options and examples
; https://docs.platformio.org/page/projectconf.html
[env:genericSTM32F411CE]
platform = ststm32
board = genericSTM32F411CE
framework = arduino
upload_protocol = dfu
build_flags =
-D PIO_FRAMEWORK_ARDUINO_ENABLE_CDC
-D USBCON
-D HSE_VALUE=8000000When the code runs it basically doesn't find any I2C devices connected.
Since this is my first time working with STM32 it's i made some mistake for sure, but i can't spot it.
Any help would be apreciated.
Solved! Go to Solution.
2025-08-27 5:22 AM
Unfortunately i don't have access to an oscilloscope right now and getting one sounds like a big investment right now. Do you kwno any cheaper models (under 150 bucks) on amazon that i can get for a few weeks and then refound after?
2025-08-27 6:54 AM
You might get used oscilloscope for relatively cheap.
But what I especially meant were logic analysers. Starting with a simple 8-channel DIN device like this: https://sigrok.org/wiki/MCU123_Saleae_Logic_clone
You can get similiar (compatible) devices from all sorts of electronics distributors, including Amazon, for 10 to 20€, or even less.
This site ( https://sigrok.org/wiki/Main_Page ) provides free PC based software as well.
I'm using it with Sigrok/Pulseview under Linux.
As a bonus, this software comes with protocol decoders for all the standard stuff, including RS232, SPI, and I2C.
2025-08-27 8:37 AM
@Ozone wrote:But what I especially meant were logic analysers.
But it's important to also be able to see the "analogue" domain.
I'm sure there must be low-cost devices available...
Here's a Raspberry Pi shield:
https://cpc.farnell.com/whadda/wpsh206/oscilloscope-board-raspberry-pi/dp/SC19412
It only goes up to ~100kHz, but that should be OK for slow I2C.
A USB pen-like "oscilloscoe" for £32:
https://thedebugstore.com/products/penscopedaq-usb-oscilloscope-rk-system-uk
2025-08-27 10:43 PM
> But it's important to also be able to see the "analogue" domain.
> I'm sure there must be low-cost devices available...
You are for sure right.
But I won't judge over other people's budget, nor do I know the specific market in his country.
At least here are some relatively cheap oscilloscope-like products below 100€ available, limited accordingly in bandwidth, channel number and features.
2025-08-28 1:03 AM
Thanks everyone for the suggestions: i found a used Hanmatek DOS1102 that should get outside my door in about 10 days (that's unfortunately what you get as delay time when buying second hand).
When it arrives i will start some more serius debugging
2025-08-28 11:35 AM - edited 2025-08-28 11:37 AM
Hey everyone, i wanted to tell you that a solution has been found: a person on the PlatformIO Forum found an error in my code: basically i was using the wrong command to assign I2C pins to the microcontroller GPIOs in the platformio.ini file.
This is the updated and working version:
; PlatformIO Project Configuration File
;
; Build options: build flags, source filter
; Upload options: custom upload port, speed and extra flags
; Library options: dependencies, extra library storages
; Advanced options: extra scripting
;
; Please visit documentation for the other options and examples
; https://docs.platformio.org/page/projectconf.html
[env:genericSTM32F411CE]
platform = ststm32
board = genericSTM32F411CE
framework = arduino
upload_protocol = dfu
build_flags =
-D PIO_FRAMEWORK_ARDUINO_ENABLE_CDC
-D USBCON
-D HSE_VALUE=8000000
-D PIN_WIRE_SDA=PB7
-D PIN_WIRE_SCL=PB6Here is also a link to the conversation on the other forum where everything is explained more deeply.
Thanks everyone for the support and see you next time
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.