2003-04-15 10:27 PM
i can not erase or write to the secondary flash
2011-05-17 2:53 AM
I'm programming Flash Loader IAP for uPSD3200 family chip .
In the VM registerthe configuration is for Boot_Code and Flash_Data. I succeed to erase and write all the sectors in the main flash .All the sectors of the main flash reside in addresses 0x8000-0xFFFF . My problem is that i can not erase or write to the secondary flash (32k)-flash boot which is the common area . When i'm using the upload option of the JTAG FlashLink in the PSDsoft Express and dumping the flash boot into a file i see at the beginning of the file the following intel-hex format record : :020000024000BC Which means that the flash boot resides in addresses of 0x40000-0x4FFFF . Is that correct? How do i access the flash boot addresses for erase and re-program?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.