2007-05-25 3:37 AM
Hypertermial received strange data not as expected in baud rate 19200!
2007-04-23 2:37 PM
thank you,
It works in UART polling sample code! in bps 9600 , the hyperterminal responds characters as I typed! But when I configure as 19200, the hyperterminal responds data not as I typed, for example, I press ''Enter'' 4 times, the hyperterminal responds as 2 question mark ''? ?'' !? anything wrong?2007-04-25 7:06 AM
Could you please precise:
Which product? on which boards? which example used? thanks.2007-05-24 10:27 PM
thank you for reply
basically the clock must be adjust to higher ! then the UART of PC receiving should be OK, the STR711-SK/IAR tool set and the UART sample code is used , the RCCU sample code must also combined with UART sample code to ensure it works also in high baud rates!2007-05-25 3:37 AM
hi kuni,
Do you have always configuration problems with UART communication? Regards, M3allemWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.