2013-06-10 7:48 AM
Hello everybody,
I'm programming a STM8L152C6 on the STM8L-discovery. Wanting to improve the consomption I tri to power down the HSI. For that I use the instruction// Clock source
CLK_LSICmd(ENABLE);
CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_LSI); while(((CLK->ICKCR) && CLK_ICKCR_LSIRDY)==0); CLK_SYSCLKSourceSwitchCmd(ENABLE); CLK_HSICmd(DISABLE); CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);What seems to work for some people according to the topics I read on this site. I'm switching the clock source perfectly and the HSION bit in the CLK_ICKCR is 0. But the HSIRDY in the CLK_ICKCR is steel to 1 and the HSIPD in the CLK_REGCSR is to 0. I'm not using any peripheral for the moment.
Am I doing something wrong? What could avoid the HSI to turn down?I hope someone can help me. Thank you very much. #stm8l-hsi2013-11-01 12:18 AM
CLK->SWCR = CLK_SWCR_SWEN;
// enable clock switching
CLK->SWR = 0xB4;
// set target clock source to HSE
while
( CLK->SWCR & CLK_SWCR_SWBSY );
// wait for clock switch
CLK->CKDIVR = 0x00;
// sys clock divider /1
CLK->PCKENR1 = CLK_PCKENR1_UART1 | CLK_PCKENR1_I2C;
// enable UART, I2C clocks
CLK->PCKENR2 = 0x00;
// disable ADC, AWU clocks
CLK->ICKR = 0x00;
// disable internal RC oscillators
Using STVD debugger over SWIM, looking at internal registers. After last instruction that should disable HSI, theHSIRDY bit remains set, even thoughHSIEN is clear. As a sanity check when I enable HSI as a clock out source, the HSIEN cannot be cleared as expected.
How to kill the HSI for good?
2013-11-01 7:37 AM
It looks like the SWIM module forces HSI on. Check out ''STM8 SWIM communication protocol and debug module'' UM0470. Figure 4 shows the HSI forced on as part of the SWIM entry sequence. You'll probably have to verify the death of the HSI via current measurement or some other non-SWIM means.
jdfWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.