2003-04-23 10:19 PM
how to set the VGA to support interlace?
2003-04-09 3:07 PM
I used the STPC Consumer2,testing the gdk14,
the sample/basic/vidfull to TVOUT is OK,but I searched the whole gdk14,not found a easy way to set the CRTC register to support interlace.any suggestion will help.2003-04-09 9:32 PM
Shuaiye,
The way to switch the CRTC in interlaced mode is quite simple. You just have to fill the CRTC register 0x39 with half of the register 0x0: REGHOST_SET_CRTC_REG(0x39, REGHOST_GET_CRTC_REG(0x0) / 2); Anyway, I don't think it is what you wan't to do. The TV encoder expect full frame from the CRTC and you will loose your TV output doing that. What do you mean exactly by 'set the CRTC register to support interlace'? Farfalla2003-04-10 5:18 PM
Farfalla
thank you for your answer.my problem is the video in the TV seems OK,but the video on the VGA have some sawtooth when the object in the video moving.I guessed maybe the signal is interlaced(so TV can play it) but the VGA not support it.maybe I am wrong.but I can not find the correct way to set VGA well to play smoothly video. the signal go the way like that: camera--->saa7113---->aq414---->STPC------->TV(VGA) shuaiye [ This message was edited by: shuaiye on 11-04-2003 05:49 ]2003-04-14 10:45 PM
Shuaiye,
Unfortunatly, if you would like a perfect quality on the CRTC, the problem is not as simple as switching in interlaced mode. You also need to synchronize the frame coming from the video input with the frame going out of the CRTC. This can be done by creating 3 buffers in memory and switching from one buffer to another only when a buffer is ready to be displayed. You need 3 buffers because one of the buffer is filled by the video input in the same time as a second buffer is dispayed by the CRTC. The video input and CRTC are not switching from one buffer to another at the same time and you need a 3rd buffer to be ready for a switch. To don't loose CPU time waiting for end of frames, the best is to use IRQs. We have got an example for Linux (attached to this message) if this can help you. Anyway, it is something difficult to implement. You could also try your solution to switch the CRTC in interlaced mode but you will never get the same level of quality and you won't be able to display on TV output and CRTC at the same time. Farfalla ________________ Attachments : vid3buf.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htqi&d=%2Fa%2F0X0000000aXq%2FIzUUj9Z1vA5quN6znrNH3dimGiN6IhMj.XqfnK4hoEk&asPdf=false2003-04-22 9:33 PM
thank you very much.
I cannot compile the file yet,because I cannot find the directory ''pci'' in src/libhard/ in the gdk14.zip package.would you please give me some advice about it?thanks again.2003-04-23 3:21 AM
The PCI module have moved from the libreg to the libhard directory in the last version of kit.
You should download what is called 'STPC Software Development Kit v1.0' in the STPC software section of this site. This development kit replace the GDK. There is additional source code which is not related to graphics but the whole contend of the GDK is still there. Farfalla2003-04-23 3:48 PM
thx.
I build the driver step by step follow the vid3buf.txt but when I insmod the vipmod.o,it report errors: ******************************************* bash-2.05a# insmod vipmod.o vipmod.o: unresolved symbol OSAL_IORead8 vipmod.o: unresolved symbol OSAL_MemoryMap vipmod.o: unresolved symbol OSAL_IORead16 vipmod.o: unresolved symbol OSAL_IORead32 vipmod.o: unresolved symbol OSAL_IOWrite8 vipmod.o: unresolved symbol OSAL_IOWrite16 vipmod.o: unresolved symbol OSAL_IOWrite32 vipmod.o: Hint: You are trying to load a module without a GPL compatible license and it has unresolved symbols. The module may be trying to access GPLONLY symbols but the problem is more likely to be a coding or user error. Contact the module supplier for assistance, only they can help you. ************************************************ and the sample program's build also report errors: ************************************************* [hex@iServer stpckit]$ make -f MakeSmp gcc -O2 -I./include -I./src/libosal/linux -T1 -c -o vid3buf.o vid3buf.c vid3buf.c: In function `ST_MainFunction': vid3buf.c:137: warning: assignment makes integer from pointer without a cast vid3buf.c:138: warning: passing arg 2 of `HWDUMP_Dump' makes pointer from integer without a cast vid3buf.c:179: `ulDumpHandle' undeclared (first use in this function) vid3buf.c:179: (Each undeclared identifier is reported only once vid3buf.c:179: for each function it appears in.) vid3buf.c:179: warning: passing arg 1 of `HWDUMP_Restore' makes pointer from integer without a cast make: *** [vid3buf.o] Error 1 ***************************************************** I use the 'STPC Software Development Kit v1.0'--stpckit-v10.tgz and the file your attached.2003-04-23 10:19 PM
Farfalla ,
It's OK now.hehe shuaiye[ This message was edited by: shuaiye on 30-04-2003 04:13 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.