2006-10-05 1:55 AM
How to interface 16 bit data bus to 8 bit peripherals
2011-05-17 12:32 AM
We are using STR912FW42.We are planning to use 16 bit nand flash memory as EMI(external memory).So for that we kept the data bus in 16 bit mode.We are planning to use external UART for our application.How to interface 16 bit data bus from controller to 8 bit peripherals.
Regards Anuradha.2011-05-17 12:32 AM
I suggest to you to use the low 8bits D0-7
a read access to the bus is performed reading all 16 bit and the processor ignore the upper byte. EMI_RD for reading if you need write to the peripheral you have to use EMI_WRL If your peripheral has only a R/W line you need to combine with a couple of logical gate the EMI_RD and EMI_WRLWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.