2020-01-30 2:40 PM
standard IAR program. Transmit works normally ( without interrupts ).
Receiving doesn't work not with flag polling, not with interrupt. I have seen in Internet similar questions, but no one answer with reasonable explanation or unconditionally working example.
Thanks in advance.
2020-02-13 10:24 PM
Hi Ygrod!
Try to list your code, the USART works perfectly if configured correctly and it's one of the best USART peripherals out there on a 8-bit MCU. The USART_RXNE flag is set by hardware when a byte is received and ready to be read. So you can only "force" it by activating the receiver and supplying a correct byte frame on the RX pin.
Good luck!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.