2003-10-21 12:27 AM
how can I get 5V DC from 220V AC? without transformrer.
2003-10-20 10:10 PM
I am now doing a project, ( AC power, Thermal Controller )
Only allow to use mcu + thermal resistor + heater. I feel headache that the voltage supply is AC, how can I get 5V DC from 220V AC? without transformrer. Is it possible to use discrete components to do it? zener diode? cap? resistor? because the project is cost-down approach.2003-10-20 10:26 PM
Have a look at the following app notes:
http://us.st.com/stonline/books/pdf/docs/8313.pdf http://www.microchip.com/download/appnote/pic16/91008b.pdf Regards sjo2003-10-20 10:48 PM
Thank you very much ~~ that 's a good reference notes~~
but how can I calculate the current can be supported ? I am worry if it can provide enough current in high power application (temperature control)2003-10-21 12:27 AM
This type of power supply is dependent on the AC cap, the practical limit is really about 20mA.
The supply can be improved by using full wave rectification but does add cost. See schematic attached (Simetrix spice model). Regards sjo ________________ Attachments : fullwave.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Jj&d=%2Fa%2F0X0000000bXF%2Fhqpy3i_ODaIyYiwWtYSr5ZUb9.QybvjsnE.NaeWhpJA&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.