2008-03-27 9:09 PM
2011-05-17 12:50 AM
As title,
I use STR911FAM44X6, when I run flash up than 48MHZ the system hang... So I only can run it on 48MHZ... If some one knows solution, please kindly give me some advices... Thank you very much2011-05-17 12:50 AM
Dear tiffanychen,
Please verify the Flash wait states insertion when running above 48MHZ. For example when running @96MHZ, Insert 2 Wait States for read: FMI_Config(FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0, FMI_PWD_ENABLE, FMI_LVD_ENABLE, FMI_FREQ_HIGH); Kind regards, Eris.2011-05-17 12:50 AM
Hello tiffanychen,
There is no problem with running flash above 48MHz. However, the maximum PCLK frequency is 48 MHz. Please find attached a simple example of toggling leds, flash running at 96MHz, and it's working well. Please verify if you have something wrong in your software application. Best regards, Amira.2011-05-17 12:50 AM
Hello tiffanychen,
There is no problem with running flash above 48MHz. However, the maximum PCLK frequency is 48 MHz. Please find attached a simple example of toggling leds, flash running at 96MHz, and it's working well. Please verify if you have something wrong in your software application. Best regards, Amira.2011-05-17 12:50 AM
I'd already try the example from mirou,
but the system still hang... Because the example is used for STR912...not STR911 so I just copy the clock setting part on my code I also set the Wait state to 2, but it still can't run... Please give me some advices if you have any idea... Thank you very much2011-05-17 12:50 AM
Can everybody help me?
Thank you very muchWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.