2003-11-28 2:48 AM
Help me, please, with data Flash paging
2011-05-17 2:56 AM
Hello,
I have several problems with paging data Flash in uPSD3212, using DK3 Here's it: I'm gonna build two generators: one at PB0 and the second at PB1. The code is as follows: $include (reg_upsd321x.inc); describe all uPSD registers CSEG at 0 ljmp my_code_s code_seg SEGMENT code RSEG code_seg my_code_s: mov WDKEY,55H; disable watchdog timer mov IE,10010101b; enable UART0 interrupt mov IEA,00010010b; enable UART1 interrupt ; mov DPTR,802H; set pointer to a port A mode mov A,00H; set data to 0H movx @DPTR,A; port A is configured as I/O mode ; mov DPTR,806H; set pointer to port A direction mov A,00001111b; set 4-output and 4 input pins movx @DPTR,A; set the port direction register ; mov DPTR,803H; set pointer to a port B mode mov A,00H; set data to 0H movx @DPTR,A; port B is configured as I/O mode ; mov DPTR,807H; set pointer to port B direction mov A,0FFH; port B is set as output movx @DPTR,A; configure port B ; label: mov DPTR,8E0H; select page register mov A,0H; select the page movx @DPTR,A; set page '0' as current page call proc; mov A,1H; movx @DPTR,A; set page '1' as current page call proc; mov A,2H; movx @DPTR,A; set page '2' as current page call proc; mov A,3H; movx @DPTR,A; set page '3' as current page call proc; ljmp label; ;&&&&&&&&&&&&&&&&&&&&&&&&&&&&&&&&&&& proc: mov DPTR,0C000H; movx A,@DPTR; mov DPTR,805H; movx @DPTR,A; mov DPTR,8E0H; ret END I use pages 0,1,2 and 3 for paging (bits 0 and 1 in Page register). Data Flashes are difined from C000H up to FFFFH. Thus, I need to load all my data Flash segments with its own data file. I have them for each data Falsh block, thus, I don't need to change addresses in PSDSoft when merging hex-files. My hex-files are generated in the same compiler (Keil) and their textes are: for the first hex org 0C000H DB 00000000b END for the second hex org 0C000H DB 00000001b END for the third hex org 0C000H DB 00000010b END and for the fourth hex org 0C000H DB 00000011b END When programming, PSDSoft programms all data flash regions. Finally, when the program starts, I must see my two generators, where PB0 oscillates two times faster than PB1. Instead of this, I see series of short positive (relatively to negative) pulses at PB0 generator, but PB1 generator is absolutely silent. Will you, please, answer, what I do wrong and how shall I do to get the expected result? I created this project to learn paging and data flash operations. Thank you in advance.2011-05-17 2:56 AM
Quote:
label: mov DPTR,#8E0H; select page register mov A,#0H; select the page movx @DPTR,A; set page '0' as current page call proc; mov A,#1H; movx @DPTR,A; set page '1' as current page call proc; mov A,2H; movx @DPTR,A; set page '2' as current page call proc; mov A,3H; movx @DPTR,A; set page '3' as current page call proc; ljmp label; before calling PROC sub, you need to save the data pointer of Page Register, it is changed.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.