2008-04-07 9:51 PM
2011-05-17 12:51 AM
Hi,
I would be grateful to anyone who could provide a short piece of sample code showing how to write and read SSP SPI in 16bit and 9 bit format. To is to drive an SPI to MDB external chip. Thanks!2011-05-17 12:51 AM
Hello arm.nine,
Please refer to the STR750 standard library available on the net. You will find a basic example of how to use an associate SPI EEPROM driver to communicate with an M95640 EEPROM. I think the porting should be straitforward since the SSP IP is the same in the two products. I have just one comment, please take into account that the feature of managing the NSS pin by software is not available in STR91xFA. Best regards, mirouWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.