2019-01-14 2:09 AM
2019-01-14 2:45 AM
The link to the firmware provided seems to be a "short circuit": https://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-ild004fw.html
Perhaps approach ST directly (FAE or via distributor).
2019-01-28 3:18 AM
I tried to load the demo firmware from ST using ST visual programmer but I got the error below.
Error : Cannot communicate with the device !
Check the SWIM cable connection and check all the needed pin connections on the SWIM connector.
If the application code uses Swim Disable and Reset pin as Output or has disabled SWIM Clock Divider:
Try Now to SWITCH OFF and ON the application Power Supply while NRST Reset pin is forced low.
Regards,
Walter Macamos
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.