2020-12-01 10:07 PM
after add
stm8s_gpio.c and stm8s_gpio.h and build project, the compiler(Cosmic) tell error
#error cpstm8 main.c:25(15+3) bad struct/union operand
#error cpstm8 main.c:34(14+3) bad struct/union op
2020-12-01 10:09 PM
#error cpstm8 main.c:25(8+5) GPIOA undefined
it's look like somethings not define to project.
here is remaining part
Help please.
Code:
25: sw = GPIOA->IDR & 0x06;
34: if ((GPIOA->IDR & 0x02) == 0)
sw = GPIOA->IDR & 0x06;
2020-12-02 10:01 PM
Have you included <stm8s.h> ?
2020-12-02 10:12 PM
when i include stm8s.h
it show error like this.....
#error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:211(26+6) redeclared typedef int8_t
#error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:212(26+7) redeclared typedef int16_t
#error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:213(26+7) redeclared typedef int32_t
#error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:216(26+7) redeclared typedef uint8_t
#error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:217(26+8) redeclared typedef uint16_t
#error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:218(26+8) redeclared typedef uint32_t
#error cpstm8 main.c:9(13+12) missing )
#error cpstm8 main.c:9(23) missing )
#error cpstm8 main.c:27(2+10) GPIO_Pin_1 undefined
9: unsigned int PBSW,PBSW1;
27: PBSW = GPIOA->IDR & 0x02;
/*!< Signed integer types */
211; typedef signed char int8_t;
212: typedef signed short int16_t;
213: typedef signed long int32_t;
/*!< Unsigned integer types */
216: typedef unsigned char uint8_t;
217: typedef unsigned short uint16_t;
218: typedef unsigned long uint32_t;
line 211-218 are available in stm8s.h file
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.