2018-07-24 3:59 AM
Solved! Go to Solution.
2018-07-29 11:45 AM
Well, there is table 42 with the descriptions. The one for jrf states "never jump". The instruction set entry for nop (which is separate from jrf states "see also: jrf").
It might be there for orthogonality. The reasoning for including such an instruction in the HC08 / S08 architecture was that the jrf can be used as a placeholder for a jra to some debug instrumentation code (so the debug build would have the same code locations as the non-debug build).
An interesting aspect of jrf is that it is essentially a two-byte nop for any second byte. If you put a valid 1-byte instruction into the 2nd byte, you could see jrf as a jump over that 1-byte instruction (saving 1 byte over using a jra). That can be useful in a if/else, where the else consists of just a 1-byte instruction. SDCC actually uses jrf for such an optimization.
Philipp
2018-07-26 12:31 AM
jrt (which is more commonly called jra) is a relative jump instruction. It can only jump to nearby targets, takes 2 bytes and 2 cycles. jp is an absolute jump, that can jump to anywhere within a 16-bit address space. It takes 3 bytes and 1 cycle.
So in cases where you could use either it is a trade-off between code size and speed.
For more details see the "STM8 CPU programming manual":
https://www.st.com/resource/en/programming_manual/cd00161709.pdf
Philipp
2018-07-29 7:55 AM
Yes, it's understandable. I read the manual, but unfortunately it is very short.
I thought a lot about what a would mean to False or True in the "Condition" column for instructions JRT and JRF.
Ok, JRT it's alias for JRA.
What is JRF? Alias for NOP?
2018-07-29 11:45 AM
Well, there is table 42 with the descriptions. The one for jrf states "never jump". The instruction set entry for nop (which is separate from jrf states "see also: jrf").
It might be there for orthogonality. The reasoning for including such an instruction in the HC08 / S08 architecture was that the jrf can be used as a placeholder for a jra to some debug instrumentation code (so the debug build would have the same code locations as the non-debug build).
An interesting aspect of jrf is that it is essentially a two-byte nop for any second byte. If you put a valid 1-byte instruction into the 2nd byte, you could see jrf as a jump over that 1-byte instruction (saving 1 byte over using a jra). That can be useful in a if/else, where the else consists of just a 1-byte instruction. SDCC actually uses jrf for such an optimization.
Philipp
2018-07-30 3:40 AM
>An interesting aspect of jrf is that it is essentially a two-byte nop for any second byte.
Curious. The Reference Manual for HCS08 for the BRN has a more detailed description:
"This instruction can be useful in instruction-based timing delays. Instruction-based timing delays are
usually discouraged because such code is not portable to systems with different clock speeds."
Does this have a relationship with STM8? I don't understand how to make a delay on the basis of JRF or BRN instruction.
;code of delay 1sec without JRF:
stm8/
segment 'rom'
; delay 1 sec, when fCPU=2MHz
.delay:
ld a, #$06
ldw y, #$1a80 ; 0x61a80 = 400000 i.e. (2*10^6 MHz)/5cycles
loop:
subw y, #$01 ; 2 cycles
sbc a,#0 ; 1 cycles
jrne loop ; 2 cycles, flush
ret
endcode of delay 1sec with JRF:
stm8\
segment 'rom'
; delay 1 sec, when fCPU=2MHz
.delay:
ld a, #$03
ldw y, #$d090 ; 0x3d090=250000(dec) i.e. (2*10^6 MHz)/8cycles
loop:
subw y, #$01 ; =2 cycles
sbc a,#0 ; =1 cycles
jreq {exit+1} ; =1 cycles
exit:
dc.b $21, $81 ; JRF RET, =2 cycles, flush
jra loop ; =2 cycles, flush
endIt's has meaning?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.