2026-02-13 10:52 PM
hi all,
which firmware to use for STEVAL-STWBXCS1? datalog2 or ai monitor?
regards,
2026-02-17 6:13 AM
Hello @denim83
Both are valid for STEVAL-STWINBX1.
It depends on the use case you're addressing:
There is also a further function pack called FP-SNS-STBOX1 supporting STWIN.box. It is a collection of sample firmware examples to perform sensor and audio data reading, motion algorithm feature demo, and BLE connectivity.
The default firmware for STEVAL-STWINBX1, natively flashed onto the board, is the BLEDefaultFw example distributed in source code into FP-SNS-STBOX1.
Best regards,
Simone
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.