2006-04-11 3:33 AM
2006-03-31 2:22 AM
when ever I try to read the RC calibration value from the location 0xDEE0 and 0xDEE1, It gives the error “stopped on read protection at 0xdee0�. I am using the DVP3 emulator.What could be going wrong? I want to turn off the read protection for this location and read the calibration value from it. Kindly explain as to how to go about this.
Regards, Suganya2006-04-02 8:43 PM
Hi Suganya,
do you use the Lite2X? If so you have to select 0xFFDE,0xFFDF for calibration value. The the Lite2X's memory address of the calibration value is different to all the other Lites - Lite1X, Lite3X or LiteUS. Regards WoRo2006-04-02 8:49 PM
Hello WoRo,
No i am using the ST7FL35 micro, which is a Lite3x series. Verified with the manual regarding the address and it is 0xDEE0 and 0xDEE1 but i am still facing this error. Any clue??? -Suganya2006-04-02 10:26 PM
Hi Suganya,
even though I won't think you forgot to select the Lite35 on your DVP3 I'll make mention of it. A wrong MCU selection could be the cause of the error message. Regards WoRo2006-04-02 10:37 PM
I verified my settings and it does reflect ST7FL35 for MCU Configuration. Not sure what is going wrong.
-Suganya2006-04-03 2:45 AM
Hi again,
I found something that looks like an error of the STVD7: If you select your Lite35 and open the map (start Debugging and then open: Debug Instrument -- MPU Configuration) you'll see a reserved area from 0x0200 to 0xDFFF. That might be the bug! Please select the ROM area (0xE000...0xFFDF), modify it to 0xDEE0...0xFFDF and try again. The RESERVED area automaticly will shrink up to ...0xDEDF. Sorry, I can't test it by myself because I have no application on this micro. Best regards WoRo2006-04-03 5:10 PM
Thanks WoRo,
It worked with out the error, but the return value from the RC calibration value location is always 0xFF. Is this the calibration value stored for a 1 Mhz clock to be generated? Regards, Suganya :)2006-04-11 3:33 AM
RC calibration is not emulated with emulators (DVP3 or EMU3) because the RC used in the emulators does not need calibration as in the real MCU. The data you read in memory are not significant. You must use ICD for debugging code related to calibration values in order read actual calibration data and reproduce potential errors due to miscalibration of the RC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.