2007-06-18 10:09 PM
2011-05-17 12:44 AM
Hello ,
I have CPU version STR912FAZ42, which is packaged in LFBGA144 and so it has connected pin EMI_BCLK on output pin M8. And now the question: Did anyone bring EMI_BCLK signal into run? I configured EMI into 8-bit non-multiplexed mode, but still no clock signal running on EMI_BLCK pin. :-? See my code bellow (Note, that before calling this piece of code the CPU is configured and succesfully running and my AHB bus clock is HCLK=96MHz):Quote:
/* EMI SCU config */ EMI_DeInit(); SCU_AHBPeriphClockConfig(__EMI,ENABLE); SCU_AHBPeriphClockConfig(__EMI_MEM_CLK,ENABLE); SCU_AHBPeriphReset(__EMI,DISABLE); SCU_AHBPeriphIdleConfig(__EMI,DISABLE); SCU_AHBPeriphIdleConfig(__EMI_MEM_CLK,DISABLE); SCU_AHBPeriphDebugConfig(__EMI,DISABLE); SCU_AHBPeriphDebugConfig(__EMI_MEM_CLK,DISABLE); SCU_EMIModeConfig(SCU_EMI_DEMUX); SCU_EMIBCLKDivisorConfig(SCU_EMIBCLK_Div2); /* connect GPIO P8 and P9 to EMI block */ GPIO_EMIConfig(ENABLE); /* Init EMI */ EMI_InitTypeDef emi; EMI_StructInit(&emi); emi.EMI_Bank_IDCY = 0x1; emi.EMI_Bank_WSTRD = 0x1; emi.EMI_Bank_WSTWR = 0x1; emi.EMI_Bank_WSTROEN = 0x1; emi.EMI_Bank_WSTWEN = 0x1; emi.EMI_Bank_MemWidth = EMI_Width_Byte; emi.EMI_Bank_WriteProtection = EMI_Bank_NonWriteProtect; emi.EMI_PageModeRead_TransferLength = EMI_8Data; emi.EMI_PageModeRead_Selection = EMI_NormalMode; EMI_Init(EMI_Bank0,&emi); Thanks 8-) Jan2011-05-17 12:44 AM
Ok, I got response from ST support centre ;)
Resolving the problem with EMI_BCLK signal is simple. My configuration code as you can see in my previous post has been OK. But minimally one read or write access to EMI interface must be done before the EMI_BCLK signal is running continuously. So you can add the following dummy read command to the end of previous configuration:Code:
/* to activate EMI BCLK minimaly one read (or write) cycle must occur */ u32 emival = *(u32 *)0x3C000000; and EMI_BCLK signal is running (I can see 48 MHz square signal on oscilloscope on pin ''M8''). So the topic is closed by myself, cu in another one :) JanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.