2005-05-25 6:57 AM
2011-05-17 3:07 AM
Hey,
I'm trying to implement EEprom Emulation using CSBOOT0-3 banks. I'm following the Application Note AN2040. I can't get it to work, my code hangs. I've also managed to get the example code to hang, found here, Within the example code if I download it to the upsd3200 development board using PSDSoft, all works perfectly, but if I go back in and simply click ''Fit Design to Silicon'', the ''Merge MCU..'' without changing any paramters or re-compiling, when I download the program again, it will not work whatsover. I think this has a direct correlation as to why I can not implement this into my current program. Anyone have any ideas or care to try to see if they get the same error? Thanks, Mike[ This message was edited by: Viper21 on 25-05-2005 17:27 ]2011-05-17 3:07 AM
Well, I fixed my problem. It now works flawlessly. I'm not exactly sure of the cause, but I installed the new PSD Express 8.40 and it now works flawlessly. I was using PSD 7.7 before. I'm not exactly sure what changes were made in the different versions, but it was enough to affect the eeprom emulation code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.