2005-03-30 7:23 PM
2011-05-17 3:06 AM
Hello,
I would calculate a duty-cycle usig the programmable counter array but I have confused ideas can to indicate some example to me TKS2011-05-17 3:06 AM
The interrupt vector for uPsd33xx identifies all interrupt and it is declarer in ups3300.h however the pca interrupt is the number 11
2011-05-17 3:06 AM
hi,
assumed that you consider ''all-high''=0% and ''all-low''=100% duty-cycle (''active-low''): duty-cycle = CAPCOM_value / (max_counter_value+1) if you consider ''all-low''=0% and ''all-high''=100% duty-cycle: duty-cycle = (max_counter_value+1 - CAPCOM_value) / (max_counter_value+1) where: max_counter_value+1 = 2^8 for 8-bit-PWM, 2^16 for 16-bit-PWM (see datasheet: the output is high when the PCA-counter equals or exceeds the CAPCOM-value)2011-05-17 3:06 AM
I have the same problem,
I'm new to the uPSD, I have a DK3300 board and I want to interface a 2-axis accelerometer with PWM output, so my need is to decode the PWM ratio coming from an external signal. My problem is the configuration for the interrupt vectors;I can configure the registers following the user manual, but where do I define the interrupt vectors for the PCA? thank you very much! :-[We’re moving the ST Community to a new platform to give you a better and more reliable community experience.