2004-03-17 10:26 PM
2004-03-09 12:48 AM
Are Windows CE.net, XP Embedded and QNX drivers available for the Vega yet? If so where can they be downloaded from, if not what does the roadmap look like?
TIA, A.2004-03-17 10:26 PM
Hi
That's a good question... I have partially the same. My experience with the STPC-VEGA- EVALBOARD: WindowsCE4.2 Missing driver for network driver (ste10/100 on pci, with the integrated even more), had troubles with graphic driver (LynxEM4+) but there the ddi-flat works fine. XPe If you use the Target builder with SP1 you have to upgrade to SP2 (exchange ntoskrnl.exe). XPe is running, but quite slow. Maybe not one of the best OS choice for this processor. QNX Good question. Does someone have experience? The consumer- processors are covered by the qnx bsp 'x86', also the vega (a normal pentium2, like Intel?)? What's about the ste10/100 network driver? Chris [ This message was edited by: chris_s on 18-03-2004 15:53 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.