2005-11-21 9:44 PM
disabling/enabling interrupts, but with condition
2005-11-20 9:33 PM
Hello
I saw somewhere, but I don't remember where :( , a sample of code that does something like this: ints_enabled = interrput_status ..... //code if ints_enabled enable interrupts. It was a very short (assembly, I think, source) Can anybody help me restore it ? thanks Oren2005-11-20 11:18 PM
otmaza,
to test if the interrupts are enabled (condition code register flag I=0) there are two assembly instructions: JRM and JRNM. The former jumps to the destination label when interrupts are enabled, where the latter jumps when interrupts are disabled. However, I don't know how to translate these assembler instructions in your C compiler... Bye EtaPhi2005-11-20 11:44 PM
Nice :)
I didn't notice those instractions. Do you have example of assembly code ? (I will see how to merge it to my C code) Thanks Oren2005-11-21 12:47 AM
Hello Oren.
I use only assembler when programming ST micros, so take my reply with a grain of salt... The JRM and JRNM istructions alter the execution flow, so they can not mixed with C statements. However my little contribution is an asm routine which returns the I state. Its prototype is: bool AreInterruptsEnabled( void ); Its asm body is:Code:
AreInterruptsEnabled LD X,S CLR A JRM WriteResult CPL A WriteResult LD ($102,X),A RET I think that it is all you need... EtaPhi BTW: My routine is untested. It makes these assumptions: - the caller pushes one byte on the stack for the result - the caller pops the result form the stack - the stack is located in page 1 If the C compiler uses different calling assumptions IT CRASHES VERY BADLY.2005-11-21 4:12 AM
Hello EtaPhi
Thanks a lot for the help! I wonder if you can tell me what is the S register in your code. Is it the SP register ? Why is the indexed is $102 ? What is page 1 ? (I only know that there is page 0 for short access, and the rest (for long access)) do you mean - not page 0 ? Also when you wrote the caller pushes one byte on the stack for the result you mean that is one C routine parameter ? And ''the caller pops the result form the stack'' do you mean that the results always return in the stack, and not in register A ? Thanks a lot Oren Anyway, it gave me direction....2005-11-21 7:24 PM
Hello Oren.
Here are the code explanations.Quote:
I wonder if you can tell me what is the S register in your code. Is it the SP register ? Yes, S is the lower byte of the stack pointer.Quote:
Why is the indexed is $102 ? The stack area is generally mapped at the upper zone of page 1, i.e. downwards from $01FF. When the LD X,S executes, the top stack contains the caller address (two bytes). LD A,($100,X) reads the top stack value, which is the first unused location. If one wants to read the first byte before the return address, he/she must add 3 to S, because S+1 contains the lower byte of return address, S+2 contains the higher byte and S+3 contains the byte that was pushed by the caller. BTW, I made an error: LD ($103,X),A - not LD ($102,X),A - sets the result...Quote:
What is page 1 ? You know what page 0 is. By extending this idea each block of 256 bytes is generally called page. According to this definition, the page number is equal to the HIGH byte of the block address.Quote:
Also when you wrote the caller pushes one byte on the stack for the result you mean that is one C routine parameter ? And ''the caller pops the result form the stack'' do you mean that the results always return in the stack, and not in register A ? The calling convention is compiler specific. My code uses one convention which may not be what your compiler expects. If the result is returned in A, then the code becomes simpler:Code:
AreInterruptsEnabled CLR A JRM ReturnInterruptsState CPL A ReturnInterruptsState RET Regards, EtaPhi2005-11-21 9:44 PM
EtaPhi
Thanks a lot. You were very kind, and helped a lot. Yours Oren (I use Cosmic compiler, so I will search now for theconvention of the compiler in the Cosmic documents :) )We’re moving the ST Community to a new platform to give you a better and more reliable community experience.