2004-08-26 10:23 PM
2004-08-12 12:16 AM
Hello,
I am a little confused over the ordering codes for the ST7MDT20-DVP3 and ST7MDT10-DVP3. As far as I can see, if I order an ST7MDT20-DVP, According to the user manual I will get the following: A base MEB, a TEB for the 521/321, and an SDIP32 and SDIP42 connectors. So if I wanted to work with the TQFP64 (14x14) then in addition to ordering the ST7MDT20-DVP3 I would have to order the ST7MDT20-T64/DVP also. Now, I also want to work with the FLITE devices as well. So I now will order a TEB for my FLITE, because I already have an MEB from the ST7MDT20-DVP. So I will order an additional ST7MDT10-TEB/DVP. My first question is will I get a default DIP16/SO16 kit with the TEB, or will I have to order this seperately? (ST7MDT10-16/DVP). My other issue is that in the user guide for the ST7MDT10-DVP indicates that I must specify a connection kit option that accompanies the DVP. Which appears contrary to when ordering the ST7MDT20-DVP? Can anybody shed any light on this? All the best, Marty.2004-08-19 10:14 PM
hello,
>So if I wanted to work with the TQFP64 (14x14) then in addition to ordering >the ST7MDT20-DVP3 I would have to order the ST7MDT20-T64/DVP also. Yes >So I will order an additional ST7MDT10-TEB/DVP. My first question is will I >get a default DIP16/SO16 kit with the TEB, or will I have to order this >seperately? The ST7MDT10-TEB/DVP like the ST7MDT10-DVP3 include by default a DIP/SO package (DIP16/SO16 for ST7MDT10-DVP3) >My other issue is that in the user guide for the ST7MDT10-DVP indicates >that I must specify a connection kit option that accompanies the DVP. >Which appears contrary to when ordering the ST7MDT20-DVP? the connection option ordering is the same for ST7MDT20-DVP3 & ST7MDT10-DVP3. for example if you need DIP32/S032 you have to order ST7MD10-32/DVP. Regards2004-08-26 10:23 PM
Thanks Ronaldo.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.