2005-05-25 1:53 AM
2005-05-23 9:45 AM
Is a ST2732xx-EVAL (InSem eval board), SofTec Indart-STX and STVD7 using a Cosmic compiler a compatible setup?
I have provided my compiler path in the stvd7 (for indart) to point to my cosmic compiler. However starting on a new project I have no clue how to get even a hello world program running. I am new to the ST7s and have no prior experience programming for thtem. My target board is a InSem (Korea) ST2732xx-EVAL board which I have connected to SofTec's Indart programmer/debugger. Do I need to write my own make/batch file? I just need a little primer on waht is to be done. Thanks2005-05-25 1:53 AM
From STVD7 r3.0.0 and on there is no longuer the need to make a makefile or a batch file for driving the compiler/linker.
You can download STVD7 r3.0.0 for Indart at : http://www.softecmicro.com/downloads/prog/st7_toolset.exe Please refer to example provided for Cosmic. Best regards AlainWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.