2005-05-10 11:29 PM
2005-05-02 10:30 PM
Hi all,
I would like to ask if the debugger has the ability to record the steps that have been run in the program to trace back the statements that have been executed? Pls advice. Rgds, TH Ong2005-05-03 3:09 PM
Hi,
Thanks for the info. Well,its going to be tough searching for a bug without this functionality. Rgrds, TH Ong2005-05-03 5:33 PM
Hi again,
Does Realview Trace provide the profiler functionality that I've wanted? Im using RealView Ice. Rgrds, TH Ong2005-05-10 7:50 PM
Hi,
using RealView ICE does not necessarily mean using RVDK, as the JTAG-Adapter shipped with RVDK is referred to as ''RealView ICE Micro Edition''. The RealView ICE is a tool that can be used with RVDS as well, connected to USB or Ethernet. @ongth: I guess RealView Trace provides the needed functionality regards, MarcusWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.