2008-04-16 9:37 PM
2007-05-21 4:36 AM
Hi. At what moment debug/readout protection becomes valid (takes effect)? Is it immediately after writing the appropriate register or some additional action is needed (e.g. device reset)? Thanks for the answer.
2007-05-21 5:41 AM
Hi opijozko,
Yes, the debug/readout protection becomes valid immediately after writing the appropriate register. Regards, Najoua.2008-04-14 11:33 PM
Hello,
I looking for readout protection of my code. Im using a STR712, IDEalist and the wiggler to program it. Usually I just tick a box to readout protect the code, but for the ARM it looks like it is not that easy. Could someone tell me the easiest way to protect my code ? Regards, Alex PS: The hardware is done and can't be changed.2008-04-15 2:46 AM
Hi alexandre.o
I don't know the IDEalist and it's features. However, readout protection feature is implemented for our universal device programmers (JTAG interface is used for in-situ programming). May be, you will find them useful. See my homepage for BeeProg+ :)2008-04-15 3:59 AM
Thanks for your help opijozko.
I've been looking on your software, it is written that if I Debug/Readout protect it, I wont be able to access to my device again. But what I am looking for is to be able to program/erase only but still be able to program it from the JTAG Wriggler. Does the ARM has this possibility ? Thanks, Alex2008-04-16 9:37 PM
Hello alexandre.o.
After enabling debug/readout protection, JTAG port is disabled internally in device logic. It is not possible to use that interface, not regarding the tool or STR7xx device. However, you can still assign a part of flash memory for your own IAP bootloader that communicates e.g. via UART. Then you can use a technique described in STR7 Family Flash Programming Reference Manual for treating the debug/readout protection enabling/disabling. I'm afraid, it is the only way to solve your problem using STR71x device. For STR73x - the situation is similar. But I didn't test the system memory boot mode for this device. May be, there is some way how to erase flash and disable the protection. For STR75x there is a built-in bootloader for system memory boot mode. This bootloader enables you to erase flash and disable the protection, it communicates also via UART. Regards JozefWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.